Bus cable for the energy chain

Sophisticated bus solution for high data transfer

As automation has expanded over the past few years, data transmission requirements have risen steadily. Distances across which data is moved from sensor to evaluation unit are simple 1:1 connections. Data cables used to handle this. Now they are being replaced, bit by bit, with bus systems, which allow faster, more complex communication within the system. It requires the associated bus cables, which are good at transmitting digital signals with their steep flanks. These cables are, so to speak, special data cables that are built specifically for the requirements of the bus system in question. In the simplest case, this might be colour and core/cross section or certain capacitive or inductive properties that allow the necessary characteristic wave impedance. Today, these cables are the basis for familiar bus systems such as Profibus, Profinet and CAN bus, but also USB and CC-Link. We will show you the features that allow continuously functioning data transmission here.
 
Buy bus cables

Alternate text has yet to be replaced

Ethernet

Many bus systems are based on Ethernet. Well-known brands include Profinet, CC-Link IE, EtherCat and Sercos. They are all based on a structure that has been used for many years in mainframes and PCs. Ethernet is described in categories that cover frequencies and data volume capacities from 100 Mbps to 10 Gbps. The terms CAT5, CAT5e, CAT6A and CAT7 are frequently used. These cables contain two or four pairs in a shield pair or overall shield design, depending on requirements. We have prepared an overview matrix that considers the mechanical parameters in addition to the electrical parameters just mentioned.

Here you have the opportunity to experience the CFBUS bus cable as a virtual, three-dimensional model

Bus cable CFBUS.045

Profinet

Profinet is one of the most popular bus cables for use in industry. The real-time capability option and modular concept makes it eminently well-suited to a large majority of applications. igus has nine different mechanical qualities of Profinet cable, from PVC cables to PUR cables to cables for extraordinary applications such as those involving torsional movement or requiring great strength. Profinet fits into the Industrial Ethernet standard, alongside bus systems such as Sercos, EtherCat and CC-Link IE. igus is a member of the Profinet user organisation and conforms to all required market standards.
Alternate text has yet to be replaced

Alternate text has yet to be replaced

SPE

Single Pair Ethernet (SPE), the newest addition to the group of bus systems. The new bus technology was introduced in 2019 and has since progressively conquered the market. This innovation offers new capabilities for the fast-growing IIoT market. What is special here is the cable's new design: a single pair, but still with the capability of transmitting a CAT5e signal. We are working steadily with the SPE organisation on refining and standardising this technology. This technology has notable capabilities, particularly in applications involving tight installation space.

Profibus

Today, Profibus is one of the most important industrial bus cables. It was developed in the 1990s and quickly became the standard for reliability and high data quantities. The Profinet Nutzer Organisation (PNO), Germany's Regional PI Association, is concerned with technical refinement and coordination of various member companies such as igus. The cable, with its red and green foam cores, is very distinctive. igus provides chainflex Profinet cables in PVC, PUR and TPE designs for any moving e-chain application.
Alternate text has yet to be replaced

Alternate text has yet to be replaced

CAN bus

The CAN bus is extremely tough and remarkable for its robust network protocol. Its origins are in the automotive industry, and it is commonly found in industrial systems today. The special thing about these CAN bus cables is that they are available with different cross-sections as required and are used for different applications with one or two pairs. As with other bus systems, chainflex offers cables for linear chains and for torsion.

Other bus cables

Bus cables are used in a variety of applications, and bus systems for computers or consumer electronics are also commonly used in industrial applications. One example is USB 2.0 and USB 3.0, which have distinctive connectors and can often be found in industrial cameras. The same is true for DVI, a typical monitor interface. There are also chainflex solutions for these bus cables. Some applications require prominent bus systems such as INTERBUS or DeviceNet, which are part of the CFBUS bus cable family. There is also the prominent ASi bus cable, which is easily identifiable in any system because of its yellow colour and square corners.
Alternate text has yet to be replaced

What makes a bus cable a special data cable?

The bus cable's function, as it pertains to transmitting low-energy signals, is similar to that of a data cable. The key is not large current flows, but good signal transmission over the long term. It is different from a data cable because of its electrical design, which is harmonised specifically to the bus system. It also has different electrical values and mechanical design (core cross section and colour). A bus cable is a special data cable, so to speak.

Expert's tip

Bus cable in motion – what is different?

A design for a bus cable will focus on good data transmission. Data transmission depends on the arrangement of such components as shielding and cores, which determine transmission quality, since they are the basis of the cable's capacitive values. Position changes during movement, which in turn changes data transmission quality. The special design ensures constantly good data transmission properties. Is continuous high-quality data transmission important to you, or have you had difficulties in this area? We would be happy to talk to you. Just send us an e-mail.
Expert tip

Bus cables on a long travel

Our blog post on the topic

Bus cables for long travels and the alternatives

In long travels, our products have to permanently withstand a heavy load. Because as soon as we talk about long travels, the question of the maximum transmission length often arises, e.g. in the case of a bus cable.

In our blog post, we shed light on this topic and show the possibilities associated with it.


Haven't found the right one yet?


Are you familiar with our online tools?

Simply find and choose a suitable type, calculate its service life, and order it online
 
Product finder

Product finder

Get to just the right cable quickly
Service life calculator

Service life calculator

Calculate the service life of any chainflex cable
Copper surcharge calculator

Copper surcharge calculator

Calculate the current copper surcharge
chainflex configurators

Configurator for special cables

Configure your individual cable in just three minutes

e-chain

Are you still looking for an energy chain for your cable?

readychain

... or everything already harnessed?

... preferably with integrated condition monitoring?



Poradenské služby

Rád zodpovím vaše otázky osobne

Preprava a konzultace

Osobne:

Pondelí až pátek od 7:00 do 20:00.
Sobota od 8:00 do 12:00.

Online:

24h


Termíny "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "řetězy pro jeřáby", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", quot;e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus zlepšuje, co se hýbe", 73quot;igus:", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plasty pro delší životnost", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL" , "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "když se hýbe, igus zlepšuje", "xirodur", "xiros" a "ano" jsou zákonem chráněné ochranné známky společnosti igus® GmbH/kolín nad Rýnem ve Spolkové republice Německo a případně v některých zahraničních zemích. Jedná se o neúplný seznam ochranných známek (např. přihlášky ochranných známek nebo registrované ochranné známky) společnosti igus GmbH nebo přidružených společností igus v Německu, Evropské unii, USA a/nebo jiných zemích či jurisdikcích.

Společnost igus® GmbH upozorňuje na to, že neprodává žádné produkty společností Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber ani žádných jiných výrobců pohonů uvedených na tomto webu. Produkty nabízené společností igus® jsou stejné jako produkty společnosti igus® GmbH